Other Parts Discussed in Thread: UCC28220
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC28220 我对 UCC28220上的最大占空比设置有一个问题。
对于2个 FET 正向运行、Dmax 如何限制为<50%?
根据公式,Dmax 不能小于60%,如何将 Dmax 设置为小于50%?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.