请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS92513 100Hz 或200Hz 的单个 TPS92513电路线圈就像一个 cicada。 在1kHz 频率下、这会产生很多啸叫声。 VIN=24V、VLED=11V、LED 电流= 272mA。
如何消除音频噪声?
谢谢、
luci
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.