请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCD3138 您好:
另一个 UCD3138问题:我需要通过28V 输入实现非常紧凑的超高效率230W 和460W、以获得28V 输出、隔离式。 您是否有能够并联的低电压 LLC 拓扑的 UCD3138评估套件/支持文档
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.