This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[参考译文] TPS84410:TPS84410

Guru**** 2595805 points
Other Parts Discussed in Thread: TPS84410

请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。

https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/680702/tps84410-tps84410

器件型号:TPS84410

大家好、

我的客户在其设计中使用 TPS84410、原理图是数据表中的典型应用。 输入电压为5V、输出电压设置为3.3V。 问题是实际输出电压低于3.3V 的2.93V、我测试了 PH 波形、如下所示:


据我了解、VADJ 引脚上的电压应等于 Vref、即0.8V。 但是、实际电压大约为0.75V、如下所示: