Other Parts Discussed in Thread: BQ24610
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ24610 尊敬的 TI:
我已经阅读了 slua585设计 资源, 下面有一段描述
我 166.7mΩ,bq24610规范 Vrch 典型值:50mV,I 设置 Iterm=0.3A,、因此 RBAT_max=50mV/0.3A=8 Ω
对吗?
此致
无
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.