Other Parts Discussed in Thread: UCC27531
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC27531 团队:我可以使 UCC27531的接地为负、并相应地改变 IN 和 EN 信号吗?
例如:
GND=-10V、VDD=5V、
IN 和 EN=-10V 至-7V
输出=-10V 至 5V
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.