请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPSM84209 您好!
我查看的是 TPSM84209模块、但未看到该器件的最小导通时间规格。 对于高达12V 的应用、输出限制是什么? 该输入为1.8V、还是可以处理1.2V、这是最低的?
此致、
Ramon Jimenez
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.