请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TLC59116 大家好、
TLC594.0的数据表显示 VIL 的建议条件为0V~Vcc*0.3。
如果 VIL 电压低于0V 但高于最小绝对电压-0.4V、该怎么办? I2C 通信是否会失败?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好、
TLC594.0的数据表显示 VIL 的建议条件为0V~Vcc*0.3。
如果 VIL 电压低于0V 但高于最小绝对电压-0.4V、该怎么办? I2C 通信是否会失败?
谢谢