请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS2115 您好!
我想设计一种自动开关配置、使用两个5V@3A 电源。
输入 D0和 D1应该是什么为了实现这一点、数据表中的数据表并不简单、因为在图14中。 D0悬空、D1为"0"、而在第17页中、D0应等于"1"、D1应等于"0"。
谢谢
NIR
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
我想设计一种自动开关配置、使用两个5V@3A 电源。
输入 D0和 D1应该是什么为了实现这一点、数据表中的数据表并不简单、因为在图14中。 D0悬空、D1为"0"、而在第17页中、D0应等于"1"、D1应等于"0"。
谢谢
NIR