请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS60400 您好、Buddy
我想将 TPS60400用作电压逆变器,因此输出为负电压,在数据表中,输出电流为60mA,
您能否告诉我它是 灌电流或拉电流、换句话说、 当输出用作灌电流时、我能否通过电阻器将输出拉至接地?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.