Other Parts Discussed in Thread: TPS62822
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS62822 您好!
我们已针对我们的应用考虑了 TPS62822。 我想知道该器件的持续输出电流和开关电流是多少。
我们计划输出电压为1.85V。 我们能否使用应用电路中提到的470nH 电感器。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.