请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ51050B 主题中讨论的其他器件:BQ51051B
作为参考数据: tidraz7.pdf 和数据表(8.3.4.3电池充电电流设置计算)
有关选择 R (FOD)、R (TERM)、R (ILIM)、R (RECT)的规格说明过于复杂。 你能为我计算它吗?
我的操作是锂聚合物电池(100mAH、50mA 充电、20mA 放电)、系统操作使用5mA。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.