请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ25700A 如果 VBUS (引脚1)被外部电路下拉至 GND、则 VBATT 电压有效(sucn 为12V)、OTG 转换器是否可以启动? REGN 电压为6V 或0V?
希望您尽快回复、
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.