请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS7A92 为什么反馈电阻值的范围如此之大? 有些小至1.15K、有些则大至15K 或11.5K? 设置3.3V 输出时、我们是否可以使用11.5K 和35.7K 来替换1.15K 和3.57K?
谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.