请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LP8863-Q1 你(们)好
我对 LP8863-Q1有疑问。
如果我使用3.92kΩ Ω 电阻器将开关频率设置为303kHz、我认为开关频率低于300kHz。
在这种情况下、开关频率是固定的300kHz 还是小于300kHz?
此致、
横田洋三
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.