Other Parts Discussed in Thread: LP8556
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LP8556 你(们)好
我的客户有疑问。
每次激活 LP8556时、我都希望使用 I2C 设置寄存器。
写入后、没有计划通过 I2C 进行通信、SDA 和 SCL 将保持上拉至3.3V、但是否存在任何问题?
最恰当的考虑
T Kishi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.