请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TLV710 大家好、
根据时间表、我们知道 TLV7101828-Q1的每个输出可输出200mA。
我是否可以知道启用两个输出(2.8V 和1.8V)的最大电流输出是多少? 每个电流仍为200mA (总计400mA)?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.