Other Parts Discussed in Thread: BQ24232, BQ24232H
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ24232 你好
客户测试 BQ24232并确定充电终止电压为4.2V。 BQ24232的充电终止电压为4.2V、对吧?
如果没有、我们是否有任何 P2P 解决方案(Vbat = 4.35V)、因为充电终止电压为4.35V? 谢谢你。
BR
Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.