请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5176 你(们)好,先生
我看到 LM5176高侧 Vgs 超出规格
对此有任何建议?
原理图/波形/测试报告、如下所示
规格:VIN=22V,VOUT=24V
Iout = 3.75A (Vgs = 8.6V)
Iout = 0A (Vgs = 7.28V)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.