Other Parts Discussed in Thread: LM5035, LM5035C
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5035C 主题中讨论的其他器件:LM5035、
我正在尝试设计一个200V 的输入电压和一个200kHz 的振荡器频率。
此时、当 RFF 连接到输入端时、RFF 值约为7M 欧姆。
可用 RFF 值的范围是多少?
RFF 将消耗多少瓦功率?
此致。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.