请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UC2825 当我使用 UC2825作为 PWM 来运行半桥转换器以获得16V 输出时。 I 使 EA (引脚1)连接到引脚3 (E/A OUT)。 和引脚2 (EA NI)通过10K 电阻器连接到基准引脚16。 如何确定固定占空比是多少?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.