Other Parts Discussed in Thread: BQ25504
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ25504 您好!
下面是文档第7页的 BQ25504效率图。
我想问以下几点:
问题1. 对于这些图、负载电阻是多少?
问题2. 对于图1、如何将 VSTOR 的电压设置为1.8或3或5.5V? 电阻器值来实现的呢?
谢谢你。
此致、
磅
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.