Other Parts Discussed in Thread: LP5524
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LP5524 尊敬的 TI 专家:
是否可以将4通道 LED 输出连接在一起以驱动4个并联 LED,并施加 PWM 信号 以线性改变0~100mA 的 LED 电流? 非常感谢。
下面是第个问题
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.