请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ78PL116 我将 bq78pl116用于4节电池组。
我的一个失败是,我的电芯1低,2.9V,其他是3.53V。 当我尝试将电池1上的输入电容从30uF 更改为40uF 时、电池1、2、3、4变为3.3V、4.7V、0.9V、4.6V。
电芯2、3、4的输入电容为30uF。
我的问题是、输入电容如何影响电池电压?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.