请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:SG3524 你(们)好
对于以下规格、我们是否可以将 SG3524用于交流发电机?
VIN 12VDC,输出电压12VAC,1A,60 Hz ?
谢谢!
Py Tsai
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.