请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC256303 对于或 UCC256303、系统参数如下:
输出电压 :55.5V ,输出电流:10A 输出电流:555W
VIN-nom:150V、 Vin-max:180V、 Vin-min:120V、
LLC 频率为100kHz
您能否帮助为 LLC 电感器设计提供系数?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.