Other Parts Discussed in Thread: TPS51206
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS51206 数据表第5页指示当 VDD = 5V 时、S3、S5的 VLH、min 为1.8V。
我使用的 VDD = 3.3V。
当 VDD = 3.3V 时、什么是 VLH、min?
谢谢、Best、Steve
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.