主题中讨论的其他器件: TPS55340、 LM3478
输入为12V、我需要的输出为12.6V、电流限制为1A。
输出已连接:锂电池8.1V 至12.6V 范围、并联一个电阻负载。
由于电池也连接在输出端、因此需要进行电流限制。 否则、如果没有限制、电池将消耗巨大的电流
mc34063a 是否可能实现?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.