请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS2511 主题中讨论的其他器件: TPS25810
是否可以使用 TPS2511等 IC 为 USB-C 设备(智能手机)充电、最大电流为300mA?
哪种 IC 最适合这种情况?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.