Other Parts Discussed in Thread: TPS65132S
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS65132S 大家好、
客户现在正在使用 TPS65132S 来实现150mA 输出
其 BOM 为:L=2.2uH;C2=10uF;C4=4.7uF;C3=10uF;C5=20uF
他们想知道此 BOM 是否可行。
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.