请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS709-Q1 主题中讨论的其他器件:TPS709
符合通用电机的 GMW 3097。 它要求负载突降@ 34V Ri 2欧姆10脉冲间隔15秒。
我们已将33.7V @400ms 施加到 IN 引脚。 数据表中列出了最大32V 的电压。
该部件是否可以处理34V 负载突降?
Edgar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.