This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你(们)好
我正在设计一个5V 至-4V 转换器。
我运行的是 pspice 可调节模型-从 TI 下载。
反馈电阻器为75k (FB 至 VOUT)和25k (FB 至 VOUT_IBB)
当运行仿真电压为-12V、然后上升至-4V。
这是一个问题、因为 FB 到 GND 从8V (绝对最大额定值为5V)开始
请提供帮助
谢谢
或