请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS63020 您好:
我制作了典型应用的原理图(数据表中的图7)、但没有放置 R3;Vout=3.3V。
如果电源没有任何负载消耗5.38mA、但不一定等于 IQ 25~50uA?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
我制作了典型应用的原理图(数据表中的图7)、但没有放置 R3;Vout=3.3V。
如果电源没有任何负载消耗5.38mA、但不一定等于 IQ 25~50uA?
谢谢!