请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5148 您好!
我想听听 LM5148是否适合使用28V 输入以及20-24V 和15A 输出的可调输出?
那么、Vout 的变化是通过操纵反馈电压来完成的吗?
谢谢你。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.