Other Parts Discussed in Thread: LMR14050, TPS54540B
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS54540B 主题中讨论的其他器件:LMR14050、
您好!
TPS54540B 和 LMR14050的安全工作区是多少? 这些 IC 是否能够提供25W 输出功率@80°C?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.