请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:BQ25798您好、TI!
请建议 ME 直流/直流升压 MPPT 太阳能充电器 IC、用于使用为2节18650锂离子电池2S-2P (7.6V/6.4A)充电。 我的 PV 面板 Vmpp 范围为2.93V 至5.26V、VOC 范围为4.18V 至6.35V。 充电电流为1A
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.