请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS54821 您好!
在我的设计中、我使用 TPS54821从12V 转换为8V。
遗憾的是、输出电压在2V 左右无法稳定、而在8V 左右
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.