主题中讨论的其他器件: TPS54JA20
您好!
能否提供以下条件的效率曲线? 谢谢。
输入电压=12V
VOUT=1.8V
Fsw:600K/800K/1MHz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好、Jim、
以下是 TPS54JA20的效率仿真结果、其中显示了最大负载(12A)下600kHz、800kHz 和1MHz 条件下的所需值。
600kHz 91.3%的效率:
电感值:560nH

800kHz 90.5%效率:
电感值:560nH

1MHz 89.4%效率:
电感值:330nH

TPS54JB20的电感器值:
600kHz:470nH
800kHz:400nH
1MHz:270nH
此致!
卡兰