TPS54561的电路如下所示、使用过程中出现问题
[问题]
- SW (9引脚)<-> GND 短路
- 如果您在修复过程中移除 tps54561 ,输入/输出电路正常。
输入/输出规格如下:
输入:SMPS 48V@20A
输出(负载):12V@3~4A

问题1. 是否有任何示例会导致现在出现同样的问题?
问题2. 是否有任何情况与问题表现出相同的症状?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.