请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LM5156 大家好:
对于 LM5156、如果我想将其用作升压/SEPIC 拓扑、并且我的输入电压范围可以为12-56V、而我想要的输出为57V、那么如果我的输入非常接近输出(例如56V)、这会是个问题吗? 如果是、升压转换器或 SEPIC 都有问题、还是其中一个不有问题? 谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.