请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:USB-PD-CHG-EVM -01 主题中讨论的其他器件:BQ25792
您好
如果施加4.3V 电压、由于 TPS25750D 和 BQ25792指定的最大 I2C 线路电压为4V、因此是否存在损坏芯片的风险?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
如果施加4.3V 电压、由于 TPS25750D 和 BQ25792指定的最大 I2C 线路电压为4V、因此是否存在损坏芯片的风险?