请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
主题中讨论的其他器件:LM5155、 LM5177、LM5176 Helllow,
我想使用 SEPIC 拓扑实现以下几点。
-输入电压:24V
-输出电压:18~26V (变量)
-输出电流:5A
我曾尝试使用 LM5155QDSGRQ1、但输出电流高达2A。
请推荐支持高达5A 电流的直流/直流稳压器。

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.