Other Parts Discussed in Thread: LM5155, LM5156
主题中讨论的其他器件:LM5155、 LM5156
尊敬的:
客户想要找到电源。
输入为12-15V、输出为正负10V、输出电流可达到3A、并且内置了整流器。
特定应用是在一个板上使用两个相同的芯片、一个输出为正10V、另一个输出为负10V。 客户之前使用的特定型号是 LT1766。
请询问是否有相应的模型建议
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.