1、电池在1A 放电周期内(每容量减少1%,停止放电,10分钟再放电),放电到附近的截止电压, SOC 概率跳到0 (24%跳到0%)。 这是一种正常现象吗?
2.在10°环境中、电池1A 持续放电时 SOC 跃升几次(12%跃升到99%、14%跃升到99%)、可能的原因是什么? 如何解决该问题?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
感谢您的回复!
已添加#2的日志,请检查它。