请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:UCC28C43 您好!
自 PCN 20221216002以来的 UCC28C43数据表中指定了 Vref VOH 的最小值为 PCN-0.2V。
1.这种情况的典型值或最大值是多少。 您能否确认最大电压在旧典型值6.8V 的基础上现在为5V?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.