Other Parts Discussed in Thread: LMR66430
请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:LMR66430 您好
我的客户要求在 Vout = 3.3V @ 250uA 或 5V @ 180uA 的条件下、
输入电压为12V、需要低于100uA。
我是否可以检查 LMR66430是否可以满足该要求? 谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.