请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:BQ78350-R1 主题中讨论的其他器件:BQSTUDIO
工具与软件:
大家好!
SLUUBD3E (9.1.5)显示电池电量低单元为0.01%,因此7%的默认值为700。 但我检查和看到7.00不是700,哪一个是正确的? 我应该在注册表中写入什么以使其达到5%? 500或5?


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具与软件:
大家好!
SLUUBD3E (9.1.5)显示电池电量低单元为0.01%,因此7%的默认值为700。 但我检查和看到7.00不是700,哪一个是正确的? 我应该在注册表中写入什么以使其达到5%? 500或5?