请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS62933 工具与软件:
嗨、团队:
我是 FAE Jayden、我的客户对 tps62933有疑问。
从数据表中可以看到、12V 的 LC 表如下所示:

此器件能否支持2.2uH 电感器来实现 Vin=19V、Vout=12V 和 Iout=3A?非常感谢。
BRS
Jayden
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.