请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS54202 工具与软件:
许多 TI 降压转换器可以设置为反相降压/升压、例如随附文档中的 TPS54202。
我如何知道一个降压转换器是否可以设置为反相降压/升压、任何用于指示的特定功能、例如:控制模式、开关频率、轻负载行为…
因此我们可以这样说:"如果转换器为 PCM 模式、那么很可能将其配置为反相降压/升压"。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.