请注意,本文内容源自机器翻译,可能存在语法或其它翻译错误,仅供参考。如需获取准确内容,请参阅链接中的英语原文或自行翻译。
器件型号:TPS74801 工具与软件:
尊敬的 TI 专家:
对于 TPS74801、如果在输入侧耦合了一个1kHz 噪声以及非常形状的上升/下降速率、TPS74801能否抑制此输入噪声并实现干净的输出电压?
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.